Hi fellow engineers,
I have some doubts about my solution.
My problem is : I need to power LTE Cat1 modem. There are 2 power sources: external 8 to 36V DC or internal Li–Ion battery pack with min 6800mAh.
What I expect: Normal operation is modem power from external DC source. If external pwr is lost modem should continue to work, powered by the battery. (Preferably integrated switch in the charger) When external pwr is back battery pack should be charged at 500mA–1A.
Modem requirements are: 3.8V, 1A peak in LTE mode. Model is Telit LE910EU v2
Current setup is : TPS54240 (Buck) + BQ24072 (charger)
I still can't choose proper Buck/Boost for the modem and worry about performance of Buck+Charger combination.
Can someone suggest good solution for this?
If I've missed some needed information –please ask and I will try to follow up.
Thank you all in advance.