Other Parts Discussed in Thread: BQ24298, , LM3668, TPS63010, TPS630252, TPS62130
There is certainly no lack of power options for battery-powered devices (and that's just from TI)! I have two different use-cases that I'd like to get some guidance/feedback on:
1) Rechargeable LiPo powered device
2) Primary-Cell powered device (using an of: 2x1.5V Li-FeS2; 1x3V Li-MnO2; 1x3.6V Li-SOCl2)
In both cases, the desired working voltage is 3.3v, typically under 100mA with short bursts of up to 1200mA (both devices include a radio transmitter).
The LiPo device has a simpler power requirement, because the discharge curve of the LiPo battery never drops below 3.3v, but I also need a charger, so maybe something like a BQ24298 (although this isn't ideal, as my available charge voltage is 12-14v) with an LDO on its output to provide clean 3.3v?
The primary-cell device has some configurations where the battery voltage will always be below 3.3v and all configurations where the discharge curve will take it from 4.2v to under 3.3v, so in this case, I've been exploring two options: 1) a buck-boost converter like the TPS63001 or LM3668; and 2) a boost-only converter, with pass-through when the battery voltage > 3.3v, plus an LDO to regulate to 3.3v. I've seen various references (one from Maxim) that show applications where the second option is more efficient (but that admittedly comes with a lot of specific "requirements").
Thank you in advance.