Other Parts Discussed in Thread: TPS61089
Hi,
I'm using a USB power supply adapter which can deliver up to 3 Amps with 5V. When the USB power supply is not present, my system should be powered by a LiPo Battery. My average power consumption should be around 0.5 Amps, but I can get rare bursts of energy (thanks to LTE), which are around 2.5 Amps.
Hence the question - what is the max. current BQ25896 can deliver? I am totally confused by the datasheet, since I have no experience with batteries. It it the same as the max charge current? If not, do you have another part, which could deliver 3A peaks from a battery?
Regards,
Den