Other Parts Discussed in Thread: TPS61169, TPS61161, TPS61500
Hi Team,
Our customer would like to use TPS61158DRVR at the following conditions.
<Our customer’s conditions>
-VIN=4.5V
-VOUT=9.6V
-IOUT= around 200mA
-L= 22uH (TBD)
I calculated “IOUT_max” using " calculating formula(5) in the datasheet".
-IOUT_max=around 168.5mA @ ILIM(min)=0.5A
-IOUT_max=around 208mA @ ILIM(typ)=0.6A
However, according to the datasheet, the recommended operating condition of IOUT is 30mA(max).
So, can TPS61158 not output the load current(IOUT) more than 30mA?
Regards,
Kanemaru