This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: correct settings for my battery pack

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQ34Z100, BQSTUDIO

5cell_3000.gg.zipHi. i have an 5cell LiIon Pack (SAMSUNG ICR18650-30B) with an protection pcb mounted.
I am not an Battery Guru, maybe someone can check my settings?
- I find out, the cycle will never change the count on charge/discharge cycle.

- when i discharge the pack wit about 200mAh, the pack circuit will cut off about 18% capacity on BQ34Z100. The 2 red led's (10 led's config) are on

- i never get the 3000mAh if i load full. the BQStudio tells me about 2700mAh at 95%. But the charger ist finished.

I think i get a many settings wrong. But the Calibration i have made.

Many thanks