This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ76PL455EVM: COMP_UV fault

Part Number: BQ76PL455EVM

Tool/software: Code Composer Studio

Hi,

I have connected only 6 lithium ion (4.2V) cells out of 16 cells and shorted all the other to 6th cell.

I have selected only 6 channels for operation.

I have set COMP_UV threshold voltage as 2.5V. System is showing a COMP_UV fault for all 7-16 cells.

Why is it showing a fault when 7-16 cells are not selected and they are shorted to cell 6th?

Please make me understand.

Thanks

Ritul Shah