This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5529: fuel gauge bq24032 and bq27200 circuit

Part Number: MSP430F5529


Tool/software: Code Composer Studio

Hi,

I need to help for the fuel gauge circuit. The related circuit is added. My problem is the output voltage values (in my schematic, MSP_DVCC, MSP_AVCC values),

if I use lipo battery in my circuit (3.7V, 850mAh), the MSP_DVCC, and MSP_AVCC =0.6V nearly, or if I use USB connection with Microcontroller (MSP430f5529), in this case, MSP_DVCC, and MSP_AVCC =1.1 V nearly.

however, if ı measure the circuit, ı recognize that lipo battery is not charged over USB. because the battery voltage is not increased.

in my circuit, ı want to 3 volt in my output values (MSP_DVCC, and MSP_AVCC should be 3V),

What is the my error in my circuit ?

thanks for reply,

Sincerely,

5684.1.pdf7838.2.pdf