We have already successfully assembled and tested 500+ PCBs containing the TPS61046 together with a professional SMT House.
The design itself seems to be fine since we have not had any issues at all until now.
But for the next batch of 300 PCBs roughly 50% of the TPS61046 do not switch.
We find this a bit odd since nothing in the SMT process has been changed, nor any components.
The output voltage from the circuit is roughly Vin - 0.7V when the Enable pin is High (2.5V).
We have measured on the SW pin and it is not switching as compared to the working units.
We thought the problem might have been due to oxidation on the PCB, however using a lot of soldering flux and re-attaching the same IC does not work.
Replacing the TPS61046 with a new one on the same PCB does however solve the issue.
Do you have any idea what might have happened, what could have caused this problem?
It should be added that the TPS61046 is from the same batch as we used the last time and that it was about 4 months since the last SMD process.