Hi,
1>Does the BQ24650 supports simultaneous charge and discharge of Li-ion battery pack when solar power is used as input?
2>Is the BQ24650 suitable for charging a series-parallel combination of 4s30p 18650 cell battery bank using solar power as input?
3>Does the BQ24650 provides "lightning protection" when a solar power is employed as input?
4>What all protection features do I need to include, when I am planning to use solar power as input power for charging Li-ion battery pack?
Thanks and regards.