Hi,
I've got a circuit configured like the diagram below to produce two outputs, 5V and 3.3V:-
I've noticed that when operational with the shunts removed (i.e. no load attached), the voltage of LDOOut is around 4.8V and Vout is 5.4V. Have I incorrectly sized the voltage dividers at LDOOUT and VOUT? The input is a single cell LiPo battery but if I replace it with a bench supply set to 3.7V i get the same result.