Other Parts Discussed in Thread: BQ25606
HI,
We wish to use the part Bq25898 in one of our designs. Our design utilises 3000mAH battery capacity.
We are planning to use BQ25898 as a battery charger; and it will be used in standalone mode.
If BQ25898 is used in standalone mode, is it possible to achieve battery charging current higher than 2A?
What will be the default output of REGN of BQ25898 if I connect VBUS to 12VDC input?
Please suggest a battery charger (supporting standalone mode) which can deliver higher charging current to battery along with keeping all the features BQ25898.
Thanks
Rejeesh S Raj