Other Parts Discussed in Thread: BQ24780, , BQ2000
Customer is looking for a battery charger to charge 3x NiMH batteries in series (4.8V total) without having to use a host controller. BQ24780 would be a good device, but needs a host controller. Therefore we are looking for an alternative device
- supports NiMH
- with Vin from either 5V or 12V
- Power Path with automatic selection between Adapter power and battery
- Ideally supports two sources to supply input voltage
BQ24133 looks like a possible choice if it could support NiMH.
Thanks
Frank