Suppose my set charging current is 2A and corresponding to this let us say the required input current is 1.5A. If I reduce the current limit of my input source to less than 1.5 A, how will the charger behave ?? Does it continue charging at reduced current or does it stop charging altogether ?
I used a DC power supply as input and while the charging was ON, reduced the current limit of the input supply. When it went less than 1.5A, the charging was turning off almost completely. I was expecting it to operate at the availabe reduced input current but it was not happening.