This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54283: Output regulated for short time than restart

Part Number: TPS54283

Hi, i implemented a dobule dc-dc buck regulator with TPS54283.

Output 1 is 3.8V 1A, output 2 is 12V 0.6A. Input volatge is 19.1V

Here is the schematic

The input voltage is always stable but:

This is what happen to output 1:

This is the SW1 node

SW1 zoom

This is the 12V output

I tried to:

-change the boost capacitors from 100n to 33n but no improvement

-change the 100uF 16V electrolitic capacitor with 22u ceramic capacitor but no improvement

-added a 0.3A minimum load but no improvement

Please can you help me?

Thanks

Best Regards