Hello,
Regarding to PWM frequency on MC33063A, my customer is asking some question.
According to datasheet(page4), PWM frequency is a following on Ct=1nF.
(Question)
(1)Due to calculation of PWM frequency, they refered Figure1(page6) and 9.2.2.2 Detailed Design Procedure of step-up (page14).
But they couldn’t calculate it from above these information.
Could you please tell me how to calculation of PWM frequency from Ct(Timing Capacitor) in detail?
(2) About Figure1(page6),
For example, when Ct=1nF, ton time is approximately 20us.
This is meaning that ton time need to set more than 20us at Ct=1nF.
My understanding is correct?
(3) According to datasheet, PWM frequency is up to 100kHz.
I’m understanding that PWM maximum frequency as specification.
If so, could you please tell me how to lead about it with Figure1(page6)?
Regards,
Tao2199