I'm using the BQ24025 with a Varta EasyPack Li-Polymer cell (3.7V, 1000mAh).
I don't use the AC input (floating) but only the USB input.
When charging the battery with a 100mA current (ISET2 low) the status on STAT1 and STAT2 is 'fast charge in progress'. Measuring TS shows 860mV (battery at 25°C). Slow but OK.
When charging the battery with a 500mA current (ISET2 high), the status on STAT1 and STAT2 is toggling between 'fast charge in progress' and 'charge done' (500ms charging, 1000ms done). The battery voltage remains steady, not charging at all. TS is toggling as well between 350mV and 860mV (thermal alarm is issuing the toggling....).
I fear that this is due to my floating AC input.
Is it mandatory to connect AC to GND ?
May I connect AC and USB together ?