This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9248: TI Fusion startup error with new/empty device

Part Number: UCD9248


We designed a system with UCD9248 and tried to use Fusion Design Online PC Software with USB GPIO adapter.

The device itself comes with fabric hardcoded defaults (Status CMD 0x80 : => 0x24).

At the first start the device was recognized successfully, but autoconfiguration by Fusion with first simple Rail#1 required to proceed failed.

We used I2C SMB Debug to manually configure a PHASE_INFO with the 0xD2 0x01000000 command. After that the Software startup the

GUI as expected.

This autoconfiguration bug should be fixed, (if it is one).