Part Number: BQ24298
Hi,
With battery unplugged, and TS voltage input adjusted to be within range (2.5 V), STAT pin presents 1 Hz signal and REG 9 bit 0 (NTC_FAULT[0]) depicts value 1. REGN pin voltage is 5 V, input voltage is 5 V and VSYS is 3.7 V. CE pin is set high. Is there a way to reset REG 9 bit 0, stopping led blinking?
Best wishes,