This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24600: High working temperature

Part Number: BQ24600

Dear All,

     I'm facing high temperatue issue for bq24600. Chrage mode at CC and current is about 1A for a while the chip tempearuter is above 70°C.

In our layout thermal pad through via to bottom layer ground plane.  So we think it is not a layout issue.

We also measure all output signal and all signal pin  below max rating voltage .

This chip only do signal control and power mosfet is discrete why it power comsumption so high. What can i to check?

Thanks!!

Jeff Chen