Other Parts Discussed in Thread: INA168
Hi Team:
Whether this par can support Super Cap charge? If yes, could you share the schematic to me? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We do not have an actually example to share using the LM25141. But you can use a typical scheme to implement CC feedback.
Suggest looking at the INA168.
The only caveat is that the bottom FB resistor RL>5k. if the Constant voltage stage does not need to be very accurate can just use a Zerner clamp from Vout to RL Hope this helps?
The example attached is used for a boost converter, but the output current sense stage can be used on a buck topology.
Please note that the attached is only a concept. One will need to modify to suit the needs of the system and specification.
In the attached recommend depopulating Rx1 and installing the two Zeners (Vclamp voltage). Note that the output accuracy will not be precise as it will rely on the two series Vzener voltages.
Hope this helps?