Part Number: TPS62740
Other Parts Discussed in Thread: TPS62743, TPS22860, TPS82740A, TPS62746
I would like to use the TPS62740 in a design, but I can't seem to find the leakage current for the integrated load switch.
I currently use the TPS62743 and a TPS22860 load switch, which has excellent low-leakage specs, but I have to move to the TPS62740 because of manufacturing difficulties with DSBGA. Using the integrated switch would save cost and board space, but this is an extremely low power device, so I have to worry about leakage current.
Is this specified anywhere? Is there a way to find out without building prototypes (even then this isn't easy to measure)?
best regards,
--Jan
Founder, PartsBox · https://partsbox.io/ · Twitter: @PartsBoxIO