This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2844A: Very urgent question on the switching frequency of UC2844A.

Part Number: UC2844A
Other Parts Discussed in Thread: UC2844, UC2845

Dear support member,

My customer is producting UC2844A.
Very urgent.

I have two question.

1.
Regarding the switching frequency of UC2844ADTR.
Datasheet P11 Please tell me the difference from the approximate formula shown in Figure 8 (about difference from the actual)?


2.
What is the switching frequency in the case of constant below?

RT: 8.2 k (± 1%)
CT: 1 nF (± 5%)


RT: 9.2 k (± 1%)
CT: 1 nF (± 5%)

Best regard.
Bob Lee.