This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22672: Self synchronizing circuit for two devices

Part Number: LM22672


I am refreshing a design from circa 2010. This has two switchers linked so that one syncs to the others 500k clock. This has two LM22672 with directly linked RT/SYNC pins and with a single 1K pull down to 0V.  EN is not connected. This arrangement is as per the Nat Semi data sheet of that time. The new TI data sheet however shows the sync pins linked via MOSFET (switched on by one of the supplies), with two pull down resistors and also says that the startup should be controlled by the EN pin.  Could someone clarify if the new scheme is necessary or can the old method still be used?. Is it essential that the EN should both be driven from a common source?

Thankyou Rob