Other Parts Discussed in Thread: BQ24297
Customer Question:
I’m considering using the BQ24295 in a product. The product requirements:
1) Single cell, 18650 Li-Ion battery
2) Charged via USB micro B connector. I would like to utilize the USB charging port detection features:
a. USB Host or Charging Port D+/D– Detection Compatible to USB Battery Charger Spec (BC1.2)
b. Support Non-Standard 2-A/1-A Adapters Detection
3) Charging will likely be 1A rate or less.
4) Standalone operation is desired, but I2C is also fine.
Ideally I’d like the simplest and lowest cost solution that meets the above requirements. To me that looks like the BQ24295. Do you have any other parts that I should be considering?
Also, can you tell me what the difference between the BQ24295 and BQ24297 is?