This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5010: 60V to 3.3V application

Part Number: LM5010


The board power input range is 12V to 60V. I want to confirm if i can get a stable 3.3V@ 1A when i choose LM5010?

Or i need two step convertion like first get 10V by LM5010, then use another DCDC to get 3.3V?

Do you have any recommendation about the high voltage converting to low voltage application?