Other Parts Discussed in Thread: TLV61021,
Hi Sir
because i can't find "TLV61021" webench in website, may we check if we can use "TPS61021A" webench to simulation?
what's different these 2 parts?
bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, you can use TPS61021A for Webench simulation.
The only difference is the current limit point. Others are the same.
You can use this 1.2A inductor. it is OK for your application. The webench recommneds 6.7A inductor maybe because of there's not so much indcutors in their lib.
Hi
we have question about TLV61021(TPS61021A also the same) enable pin logic level question.
the datasheet show Ven_h maximum is 0.84V. is it mean if Ven_h > 0.84V, then TLV61021 will be into unexpect condition?
bogey