This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31704: 1.5, 1.8, 2.5, and 3.3V all from 500khz?

Part Number: LMZ31704


Hi Team,

Posting for a colleague. What are your thoughts for running 1.5, 1.8, 2.5, and 3.3V all from 500khz? The concern is there is only 100mV of head room for the 1.5 and 3.3V rails. With component tolerances of 2% and line transients is there any concern for being so close to the datasheet threshold?

Thanks!

Nate