Hello,
We use BQ24195 for our product, but i cannot understand the relationship between VBUS and PMID pins on BQ24195.
Based on the datasheet.
1, PMID can be used for power bank mode which will generate 5.1V if using battery.
2, There is a diode between PMID and VBUS, which means the current can go through VBUS to PMID.
3. So if the voltage on VBUS is bigger than 5V then, is there a change to damage a device that attached to PMID for charging.
4. Or it's a design rule that the VBUS shouldn't higher than 5V when using PMID for charge a device which can only bear 5V maximum?
Hope anyone can clear my questions,
thanks in advance.