Part Number: EV2300
I am having problems using Battery Management Studio and the TI EV2300 to configure the BQ34z100 fuel gauge. I am told I should upgrade the firmware on my EV2300 but the firmware upgrade process fails. I have purchased a second EV2300 and followed the procedure to update the firmware and when I click "Upload" I get an error 8. I have followed the instructions carefully and rebooted my PC several times but still no luck. I looked in device manager and I can see both the EV2300 device drivers working OK. I am using Win 10 64-bit. My EV2300 currently has firmware version 3.1c.
I have tried both these links to upgrade the firmware an both do not work for me:-
Can anyone tell me what this "Error 8" means or how I may resolve this issue? I need to resolve this problem urgently and haven't been able to get a solution so far.