This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ500212AEVM-550: Wireless power transfer with Full power mode only

Part Number: BQ500212AEVM-550
Other Parts Discussed in Thread: BQ51003, BQ500212A

Hi I want to operate the EVM module always at 110 KHz. Is it possible using BQ51003 and BQ500212AEVM.I want to disable the dynamic power correction loop I guess but how need to ask.

  • Hello

    Question-- I want to operate the BQ51003 and BQ500212A EVM modules always at 110kHz.

    Answer--This is not possible with the bq500212A transmitter, freq is changed to adjust operating point.  The bq51003 receiver will control the transmitter operating point and if the transmitter does not follow receiver command it will turn off.