Hi all
Would you mind if we ask LM53602?
<Question1>
On the P22 datasheet, it shows "This output requires a 3.3-µF to 4.7-µF, ceramic capacitor connected from VCC to GND for proper operation. An X7R device with a rating of 10 V is highly recommended."
Including DC bias, size and Temperature characteristics, does it require 3.3uF to 4.7uF?
Or, with X7R size=1206, does it require 3.3uF to 4.7uF?(actual value will be 2.7uF?)
And about Cbias, is the same as Cvcc?
<Question2>
Our customer uses the device with Vin=17V to 32V.
If Vin connects to bias pin accidentally, is the bias broken because of over absolute maximum ratings, right?
Kind regards,
Hirotaka Matsumoto