This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Product Suggestion

Other Parts Discussed in Thread: UCD3138

Hello all,

A customer is looking for an IC for the following task,

I need to generate two PWM signals (frequency 6.78MHz, duty cycle 50%) that must be shifted by an amount programmable on-line by the user (the chip will be interfaced with a micro-controller and must be programmed on-line). The PWM shift resolution (minimum shift between the two signals) must be at least 18-20 steps between 0° (signals in phase) and 180° (signals in opposite phase). I need to find an IC suitable for this task.

Could anyone help me with this?

Thank you in advance.