This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62180: The PGOOD pin only goes up to 0.56V

Part Number: TPS62180

I am using a 12V supply that the enable is connected to. PGOOD is connected to 470K pull-up to output voltage after the inductors. Vout is set be 1.1V. I tested the output for 4A load which was fine but the power good pin doesn't reach the threshold to enable other regulators.