This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: How to check EVM is working or not?

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQSTUDIO

Hi,

I am using bq34z100evm and ev2300 for I2C communication and check SOC of the battery.

6 panasonic cells 18650bl are connected in series and + (batt+) and - (batt-) are connected. I have connected a resistive load 200ohm with bat voltage 18V.

When i check on registers, SOC is 0% and max error 100%?

Why is so when battery is partially charged and sourcing a constant current to a resistive load?

Please help me out?