Other Parts Discussed in Thread: UC2844A
Hi
i am using UC2842A i.e 100% duty cycle controller for my flyback converter power output is 160W,output voltage is 450V, input is 90-264 VAc can i use this controller for this application?
presently i am testing with this controller facing problem like PWM,out put voltage is oscillating when it is coming to loop,and getting full voltage at 130Vac input with 65% load but not at 90V ac
transformer is ETD34, 35 Primary,80 Secondary turns.
same power tested with UC2844A Facing same problem that getting full 450V Out put at 140-150V ac input but not oscillating with full load with same transformer and other transformer i.e 92 secondary turns 35 primary turns. To resolve the issue of getting full out put voltage in universal input voltage changed the controller to 2842 but facing same problem with one added problem
please help me in this regards.