Tool/software: WEBENCH® Design Tools
Hi,
when I tried to simulate the design using Webench tool with following input parameters, its popping up an error"Design cannot be created with this device look for alternate device", but the datasheet shows it supports maximum duty cycle of 96%, Can you please let me know why design is not being created with below inputs in Webench tool,
Regulator1#:
Input volatge: 4.5V to 13V
Output Volatge: 3.3V
Output Current: 1A
Regulator2#:
Input volatge: 4.5V to 13V
Output Volatge: 1.8V
Output Current: 1A
Regards,
Venkat