Hi Dear,
I am using bq24133 Ic charger, my charger current does not exceed from 240mA since I used Rsense 0.01 ohm, I need PCB layout since I think that my the problem is because of my PCB layout.
Thanks in advance
Elaine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dear,
I am using bq24133 Ic charger, my charger current does not exceed from 240mA since I used Rsense 0.01 ohm, I need PCB layout since I think that my the problem is because of my PCB layout.
Thanks in advance
Elaine
Hi Elaine,
For the layout, you can refer to datasheet section 12.1 Layout Guideline bq24133 and EVM guide bq24133EVM section 4.2 Board Layout.
What is your ISET setting? Did you check the VISET? Did it follow the charging current setting shown below?
Best regards,
Ann Lien
Thanks for your response Ann,
My Iset capacitor are 32.4K and 232K which is supposed to give me about 2mA.
and the Iset voltage is 0.4.
I think something wrong is with the PCB layout, specially for current sense resistor which is not according to layout guideline in the datasheet. moreover routing analog ground is not separately from power ground...
I attached the PCB (In fact the former designer has drawn that) ,
Also I attached the new one that I am drawing and I just want to make sure that it is ok .
I was looking for a PCB layout file like bq24133EVM PCB file if it is possible.
I also should mention that our PCB has in 2 layer.
thanks in advance.
Hi Ann,
My new board received but there is no output with charger! it can switch when there is battery but it can not work with charger. Actually Vref is 3.9 which is overload but I don't know what should be the reason, do you have any idea about that?
Cheers
Elaine
Hi Elaine,
Is Vref=3.9V every time you power up? If yes, could you provide your schematic and help me to check if the IC is normal? Vref should not be 3.9V. If not, could you check the charging condition in datasheet if there is anything wrong?
Thanks,
Ann Lien