This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS735: TPS73501 Questions on Noise, Cnr and Cff

Part Number: TPS735
Other Parts Discussed in Thread: LP5912,

1) I’m used to seeing a spectral noise density plot and would like to compare noise performance of this vs. the LP5912.  Does TI have a plot for the TPS73501, or is there a way to translate the data to make an orange to orange comparison.?

2) Section 9.2.2.1 recommends using smaller resistors to minimize noise, but has a note about 2uA current which is a resistor >1.7Meg.  Is that note there just to state if you use something less than 1.7Meg, you will perform better than the fixed version? That is, it does not imply using a 1.7Meg network, does it?

3) Also in 9.2.2.1 the datasheet states a max recommended cap to be 10nF.  Is that referring to the Cnr cap, or the output cap? Section 9.2.1.1 mentions using a cap >2uF.

4) Section 9.2.1.2 requires a Cff for stability.  For the feedback network = 250k, Cff is 3pF-1nF.  I plan to use a network around 10kohm. How does the Cff range change?  Is it just scalable?