This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29910A: Maximum output power vs harmonics and 400Hz input

Part Number: UCC29910A


Hello,

We are  using the UCC29910A in a few applications, no issues there'll running between 100 and 120W. We have a fair amount of experience with this IC having worked with the Cork team in Ireland during its development some years ago as a notebook adapter. I have 2 questions;

Question 1. I am interested to know what the maximum output power could be before breaking or finding it difficult to meet IEC61000 harmonics.

Question 2. Has anyone tried this on a 115V 400Hz input supply?

Thanks in advance

Lee