This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: requirement under SEPIC configuration

Guru 29720 points
Part Number: TPS55340

Hi Team,

My customer wants to design under the following requirement with TPS55340 (SEPIC configuration).
------------------------------------------
Vin: 4.2~21V
Vout: 5V
Iout: 1A (MAX)
* using inductor that is less than 10uH is required
------------------------------------------
Is it possible to get recommended SEPIC schametic that meets the requirement?

I believe it is possible to meet the requirement with another buck-boost device but my customer strongly wants to use TPS55340 because it was already registerd in his company.
Your support would be appreciated.

Best Regards,
Yaita / Japan disty