This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for low power Buck LED driver

Guru 20090 points
Other Parts Discussed in Thread: LM3405

Hello,

Are there any LED driver which has the following specification.

Vin=4~6V, Vf=2.5~3.5V, ILED=80mA

I tried to simulate with Webench under the above conditions, but there was no matching device.
But I think that there is the device in TI.

Best Regards,
Ryuji

  • Hello Ryuji-san,

    Perhaps somebody in another group has another suggestion they will post here but of the devices I am familiar with the only one that will run to such a low voltage is the LM3405. It would provide you with a pretty small solution as it runs at 1.6MHz switching frequency.

    Regards,

    Clint