This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for an isolated, flyback solution: Input 12V-18V, Output 10.5V @ 550mA

Other Parts Discussed in Thread: LM5022, TPS40210, LM5160A, LM5160

I am searching for an isolated flyback converter design.

Input voltage: 12VDC-18VDC 

The input voltage is not variable, I can select either a 12VDC, 15DC or 18VDC as the input ti the circuit.

Output voltage: 10.5V

Output current: 550mA

Ambient temperature is around 30C may be as high as 40C