Hello all,
On the first page of the datasheet it says Different fixed voltage output versions are available from 3.15V to 5.0V.
But TPS612564C is fixed at 5.4V, so I am assuming that is just a typo.
On page 3, section 5, the table says that the minimum input voltage for the TPS612564C part is 3.3V, however on page 5, section 7.5, under VOUT for the TPS612564C, it says the input voltage can be as low as 2.3V.
Which is correct?