Other Parts Discussed in Thread: BQ25120, BQ24232
Hi,
Is there a TI charger that meets these three requirements: has DPM; OVP > 10V; and can charge at 10mA?
Thank you TI,
Roger Griswold
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David, I have a BQ24232 evaluation board, so I'll change the ISET resistor to give it a 10mA charge current and run some tests. Using the device outside its specifications is a problem, however, when it comes to production, so I'll continue to search for a device that meets the specs. Let me know if you have anything on the drawing board, I'm not opposed to designing in a future product if the timeline allows and the specs are there. Thank you, Roger