This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: Criteria A performance during surge events

Part Number: TPS2660

Hello:

I am using the TPS2660 to protect and manage the +24V power bus of my design.  Power is supplied to the unit from either an internal off-line power supply or an external 24V DC input.

In application note SLVA833 I read about the device performance during input surge events.  The circuits shown there provide Criteria B performance during surges.

Can I obtain Criteria A performance during surges using this device?  If so, how?

Thank you,

Bob Dvorak