Other Parts Discussed in Thread: TINA-TI, LM5141
I'm in the process of designing a buck converter based on the LM5141-Q1 which has some external sensing needs. Six OP-AMPS will be used to help measure input and output voltage and currents from the converter, each of which will draw a maximum of 2mA on the 5V supply to which they are connected. I was wondering if it would be possible to use the VDDA pin from the internal LDO to supply this minimal power. If not, I can add an external LDO for these OP-AMPS, but space is a serious constraint for this application, so I was hoping to source the current from the internal LDO.
As a separate concern, I was wondering if an unencrypted version of the PSpice model for the LM5141-Q1 was planned for release on spicerack, and if not, would it be possible to request one?
Thank you very much,
Ansel