Other Parts Discussed in Thread: UC3843, LM10010, DAC8811,
I need to create a 0.7VDC to 24VDC output at 8Amps for a project I am working on. The web bench can give me both the 0.7V and 24V versions, but I need to be able to feed a control voltage into the feed back loop to get 0.7 to 24V out. I have done this before with the UC3843, but the reference is too high to get down to 0.7VDC out. Is there any way to get a web bench design for this or is it just a matter of starting with the evaluation board and playing with the values to make it work?