Other Parts Discussed in Thread: , BQSTUDIO
Hi
I have a development board BQ25895EVM-664,and test it as 4.5A Charge for 8000mAh Li-lion battery,is work well, then I Design My board by BQ25895,has some issue,first my sch is this
Issue is:
1. Demo Board Temperature most can't feel,when charge current below 3.5A,but my board is very heat,most Higher than Demo board is work at 4.5A, no matter my charge set 3.5A or 2A, i had changed same inductance as demo,I try input voltage at 5V and 12V,is the same result,this is my board sw wave,and this is demo's wave ,all charge current is 2.1A,I don't no what happend
2.use ev2300 debug BQ25895,wether demo board or myself board ,when i click Battery Management studio 's "Field View",Charge will stoped ,must break off input power and battery,
3.Charger current set by ILIM,how can I calculation the resistance,such as I want set max charge current is 4.5A, the resistance value is ?
thanks !