Other Parts Discussed in Thread: LM5122-Q1, LM5122, LM5170-Q1, LM5170, LM5119
Support Path: /Reference designs/Search for reference designs/
Hi everyone.
In the last days, I've been searching some components for a project of a DC/DC converter. The requirements are: input voltage 32 up to 44 V (lithium-ion batteries), output voltage of 48V, maximum outup current of 18A. One of the IC for this project is the LM5121-Q1, and I'd like to know if this component can handle this requirements. If not, could indicate some IC that support the project?
Thank you for the help.