This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78250 Question

Part Number: BQ76940
Other Parts Discussed in Thread: TIDA-00792, BQ78350

Dear TI Team,

I am using the BQ76940 chip to make a BMS for my battery pack. the pack consists of 13 cells in series and 100AH capacity.

In the schematic the maximum output current is mentioned to be 20A. I would like to have my maximum current greater than 50A.

What are the specific changes i should do in the schematic to achieve that Or the reference design is good enough for 50A output current?

I have checked the MOSFETs, they are designed for high current (200A). the sense register is 1mOhm. it should be ok for 50A. Am I missing something here.

With kind regards,

Pratik